|
Home > Transport Equipment
|
![]() |
Brake Operating Unit for Railroad VehiclesThis system is configured as a unit with a brake operating device that plays the core role in the electric command air brake system, and the air brake valves that provide the brake cylinder pressure output for regular and emergency braking. |
![]() |
Door Operators for Railroad VehiclesComprising side-door operators and interior-door operators, the product lineup meets the needs of a wide range of applications, from ultra-low-floor light rail vehicles (LRVs) and commuter trains, to super high-speed trains. Both air-driven and electric driven systems are available. There are four door types: the pocket sliding type, the externally mounted type, the plug type and airtight doors. |
![]() |
Air Dryer for Commercial VehiclesTrucks installed with air-brakes apply the brake using compressed air supplied from the compressor, although the water content of the compressed air can cause rust and/or freezing in any equipment in the air brake system, leading to malfunctioning of the vehicles. The air dryer acts to remove any water content from the compressed air and delivers dried air into the air brake system. Nabtesco's air dryers have been adopted by all the heavy-duty truck manufacturers in Japan. |
![]() |
Brake Chamber for Commercial VehiclesIn terms of brakes, there are two types of trucks: those with air-over hydraulic brakes using a hydraulically or pneumatically controlled brake system and those with full-air brake using a full air system. The brake chamber is installed in full-air brake trucks, in which the brake is applied using the pressure of compressed air through the brake chamber. |
![]() |
Microcomputer-Aided Remote Control System for Marine Diesel EnginesThis is intended for the remote control of marine diesel engines from the ship's bridge and/or control room. It is provided with functions for the command output of marine diesel engine speed (rpm) and the monitoring of marine diesel engine conditions. |
![]() |
Engineering BusinessIn addition to products for marine vessels, the Nabtesco Marine Control Systems Company also operates an engineering business. |