TS Corporation participates in wind energy trade show in Germany. May 16 , 2004



PHOTO

PHOTO
TS corporationa subsidiary of Nabtesco, participated in "Wind Energy 2004" which was held in Hamburg from 11 to 14 May 2004. The international trade show held every other year is specialized in wind power and is considered as the largest in the world.

The company exhibited
* Yaw drive and Pitch drive based on the unique gear technology
* Intelligent yaw system and pitch system


Those products contribute to improve the efficiency and reliability of wind turbines with the following features.

* Click photo to enlarge