|
Home > Aircraft and Hydraulic Equipment Business
|
![]() |
Aileron PCU for the B777This equipment is intended for the control of the aileron. It is mounted on the trailing edge of an aircraft main wing and provides directional control of the roll of the aircraft. Typically the aileron is steered by rotating the control wheel (steering wheel) on the top of the control stick in the right and left direction. |
![]() |
Elevator PCU for the B777This equipment is intended for the control of the elevator. It is mounted on the trailing edge of the longitudinal stabilizing surface or horizontal tail plane of an aircraft and is used to obtain longitudinal or pitch-control moments. Typically the elevator is steered by moving the control stick in the forward and back direction. |
![]() |
High-Voltage DC Distribution Rack & Panel for the B787In response to the expanding need for power for aircraft use, this device supplies }270 voltage direct current (DC) power through a liquid-cooling system built into the rack. A large-capacity motor controller and an ATRU, previously installed separately, are now installed into the rack, enabling a reduction in aircraft weight due to reduced electrical wiring, in turn facilitating aircraft maintenance work. |
![]() |
GM SeriesThe GM series is used for hydraulic motors for the traveling movement of hydraulic excavators, hydraulic motors for traveling in crawlers and the wheels of crawler drills, crawler cranes and tower wagons, as well as winch driving motors for vessels and fishing
|
![]() |
CH SeriesThe CH series is used for hydraulic winch motors for truck cranes and crawler cranes, and also for hydraulic winch motors for sub-winches for forestry. |
![]() |
CS SeriesThe CS series is used for hydraulic motors for the swinging movement of truck cranes and also for feed motors for crawler drills and asphalt finishers. |
![]() |
Control Valve for Mini ExcavatorThe control valves which change the flow of oil, play a major role in the actions of oil-hydraulic excavators, including its traveling and control of the arms. This product is a sectional type multi control valve developed specially for mini excavators, and it is guaranteed to answer various needs including action control. Compact, multi-functional and with a wide range of a lineup, these control valves boastfully account for its domestic share of over 50%. |
![]() |
Drive Unit for Wind TurbinesThe drive unit for wind turbines consists of a "yaw drive (yaw gear)" to change the direction of the wind generator following the direction of the wind and a "pitch drive" to control the inclination of the blades of the wind generator in response to the velocity of the wind. Nabtesco's drive units for wind turbines are based on advanced hydraulic equipment technology and they have been favorably received in the market for their higher durability, reduced weight, compactness and other features. |